Push changes to a remote repository
    Push changes that you make to a remote repository to back up the project to a location other than your local computer and provide version control for the project. Changes pushed to the remote repository are available to others who work on the project. 
When there are changes to push, the message "Local changes are available to push" appears in the status bar and the  icon displays a blue number with the number of commits to push.
  icon displays a blue number with the number of commits to push.
Push to remote
     IMPORTANT: 
    When you push changes to the remote repository, the project must be synchronized or you will be prompted to pull from the remote repository and resolve conflicts. When there are changes to pull, the message "Local and remote changes available to push and pull" appears in the status bar and   displays a blue number with the number of commits to pull.
  displays a blue number with the number of commits to pull.  
Pull from remote
- From the open project, select.Push to remoteIf you do not have aFactoryTalk Optix Studiouser identity you are are not authorized to push changes to the remote repository.Push to remotedisplays "No identifies have been configured." SelectConfigure Provider identityand to configure the identity, see Set options.
- (optional) If version control is enabled for a local project and you are pushing changes from the local project the first time and a remote repository is not yet associated with the project, inPush to remote, configure a remote repository:- Identity. Select your identity. This can be either yourGitLab®orGitHub®identity.
- Owner/Group. Select the owner or group of the repository. This can be either your identity or a group to which you belong.
- Private. Select to create a private repository that only the selected owner or group can associate with a project.
- Public. Select to create a public repository that other owners and groups can associate with a project.
- URL. Displays the URL of the repository based on the selected settings.
- SelectPush to remoteto create a new repository or use an existing repository that is empty.
 TIP: In order to use version control, FactoryTalk Optix project names and repository names must match. The project and repository names must contain only alpha numeric characters, numerals, periods, dashes, and underscores.
The changes are pushed to the repository and "Project synchronized" appears in the Status bar.
push
backup
    
Provide Feedback