Pull preview
    Pull changes from the remote repository to see conflicts between the local project and the remote project.
The preview shows changed values and removed objects. Keep either the change in the local project or the change in the remote project. An example 
Pull preview
 may include:
      
| Item | Description | 
|---|---|
|  | Rows of highlighted conflicts or changes. | 
|  | Select  Take all localto accept all of the local changes. Select Take all remoteto accept all of the changes in the remote repository. | 
|  | Filter the changes in the preview by displaying  Allproject content, only Updatesto the project, or only Conflictsin the project. | 
|  | Select  | 
|  | Select a conflict to the left in a row to accept the local change.    Local history | 
|  | Select a conflict to the right in a row to accept the remote change.    Remote history | 
|  | An icon in a row indicates:
               
 | 
change
preview
conflict
    
Provide Feedback