Add a role
    Roles determine the responsibilities of users in a system. For example, a system may have engineering and supervisory roles.
- In the main toolbar, selectand then selectOpen dashboard pageManage users and groups.
- On the dashboard page, underRoles, selectAdd.
- InAdd Role, underName, enter the name for the role.
- (optional) If users are created, underAssign users to role, select the users to assign to the role.
- (optional) If groups are created, underAssign groups to role, select the groups to assign to the role.
- SelectAdd.TIP: To create a roles inProject view, underSecurity, right-clickRolesand then select .
The new role appears on the dashboard page and in 
Project view
.role
    
Provide Feedback