Add a group
    Groups determine the organization of a system. For example, a system may have filling and packaging groups.
- In the main toolbar, selectand then selectOpen dashboard pageManage users and groups.
- On the dashboard page, underGroups, selectAdd.
- InAdd Group, underName, enter the name for the group.
- (optional) If users are created, underAssign user to groups, select the users to assign to the group.
- (optional) If roles are created, underAssign roles to group, select the roles to assign to the group.
- SelectAdd.TIP: To create a group inProject view, underSecurity, right-clickGroupsto add a group, or select a group to add a subgroup, and then select .
The new group appears on the dashboard page and in 
Project view
.group
    
Provide Feedback