Application variables
    Bind the property of a graphic object to a predefined 
Application
 variable to configure the FTOptixApplication
. For example, bind to the visibility of a property to make the object blink based on a machine or process state.To bind to a variable, see Create dynamic links.The 
Application
 category in the Dynamic Link browser displays the variables related to the FTOptixApplication
.| Variable | Type | Definition | Read or Write | Reboot Required | 
|---|---|---|---|---|
| Blink fast | Boolean | Variable value that alternates between set for 1 second and cleared for 0.5 seconds. | Read-only | Reboot not required | 
| Blink medium | Boolean | Variable value that alternates between set for 2 seconds and cleared for 1 second.  | Read-only | Reboot not required | 
| Blink slow | Boolean | Variable value that alternates between set for 3 seconds and cleared for 1.5 seconds. | Read-only | Reboot not required | 
Provide Feedback