System object
    The 
System
 object provides the network configuration for your system through network and IP settings. Add the System
 object to access system settings such as date and time and IP addresses of the network interfaces at runtime or to restart the system. Adding the 
System
 object to your project automatically displays DateAndTime
, Device
, Display
, and Application
 property categories. Bind these properties to variables using the Dynamic Link browser.At runtime, the network interface properties are automatically added to the 
System
 object properties and display the current settings. For example, if the system has a LAN network interface that is configured with two additional IP addresses, at runtime, the System
 object properties contain a Network interfaces
 category with additional IP addresses for the LAN network. Provide Feedback