View alarms in remote local time zone
    View alarms in the local time zone to view alarm events remotely. 
- Select.Template Libraries
- InTemplate Libraries, drag theAlarm gridorAlarm history gridobject fromWidgetsinto a node in theUIfolder.
- InProject view, select the alarm object.
- InProperties, expandTimestamp.
- InText, reset the current value and then select. Change Dynamic Link Change Dynamic Link
- At the bottom of the window, selectAdvanced...
- In the Advanced Dynamic Link editor, select Insertand then selectExpression evaluator. Insertand then selectExpression evaluator.
- InExpression, enter{0} + {1}
- In the{0} DynamicLinkpane, selectand then select . Change Dynamic Link Change Dynamic Link
- In{1} DynamicLink, selectand then select . Change Dynamic Link Change Dynamic Link
- ChooseSelect.
local time zone
remote
remote time zone
    
Provide Feedback