Session nodes
    The 
{Session}
 alias points to the Session
 node for the current runtime session. FactoryTalk Optix Studio
 automatically creates dynamic links with the nodes inside of the Session
 node.Session nodes include:
        
  
    
| Node | Description | 
|---|---|
| Groups | Groups can be defined and used in the project. Each group displays a value:
                     
 | 
| MeasurementUnits | List of the available amounts. Each amount has properties based on the locale:
                     
 | 
| Locale | Array of session locale IDs. This node specifies all of the locales supported by the user interface. | 
| User | Properties for the user:
                     
 | 
| Roles | Roles can be defined and used in the project. Each role displays a value:
                   
 | 
session node
node
    
Provide Feedback