Apply a stylesheet to a report
    Use the 
StyleSheet
 property to specify an instance of the selected style to apply to the report. The units of measurement in reports are specified in 
FactoryTalk Optix Studio
 options. See Set options. The language that you select for a project determines the default unit of measurement. For example, if you set the language option to en-US
, FactoryTalk Optix Studio
 uses inches as the default unit of measurement for reports. - InProjectview, select yourReport#object.
- InProperties, inStyleSheet, select the drop-down arrow to select the stylesheet.
stylesheet
    
Provide Feedback