Recipes editor
    The recipes editor widget contains the graphical objects and NetLogics required to display and manage the recipes at runtime.
Use the recipes editor widget to:
      
- Display ingredients and values of a stored recipe during editing or loading the controller
- Create, edit, or delete a recipe
- Store a recipe in the database
- Load a recipe from theFactoryTalk Optix Applicationto the controller
- Load a recipe from the controller to theFactoryTalk Optix Application
Interface
      Recipes editor interface

| Item | Name | Description | 
|---|---|---|
|  | Recipe name | Assign a name to a new recipe or select an existing recipe. | 
|  | Recipe control buttons | 
 | 
|  | Ingredients list | Recipe schema ingredients. | 
|  | Ingredient values editor | Editable values of the recipe ingredients. | 
|  | Applied ingredient values | Values of the ingredients on the controller. | 
Provide Feedback