Edit a recipe schema
    You can edit recipe schema properties by using a dedicated interface built into 
FactoryTalk Optix
.Prerequisites
- To edit a recipe schema
- From the toolbar, select.Open dashboard page
- In the central pane, selectConfigure a recipe.
- Select the recipe that you want to edit.
- If needed, edit theNameandTarget nodeproperties.
- SelectNext.
- Select an existing database or configure a new database:- To use an existing database:- Select an existing database.
- If necessary, edit the database properties.
- SelectNext.
 
- To create a database:- SelectNew database.
- If needed, edit theNameandTypefields.
- SelectNext.
- If necessary, edit the database properties.
- SelectNext.
 
- To duplicate an available database:TIP: Duplicating an existing database allows you to create a database base on the existing database quickly.- Right-click an available database and selectDuplicate.
- If necessary, edit the database properties.
 
 
- SelectNext.
- Select the recipe parameters to use.TIP: You can show or hide variables (parameters) nested in other variables by using theNested variablestoggle. You can quickly find the parameters that you want to select by using theSearchfield.
- SelectNext.
- Review the settings.
- SelectExit.
Provide Feedback