Save a project
    Save your project to save your progress. You can store projects locally, in a version control repository, on a network drive, or a removable drive.
- Save the project using one of three ways:
- From the toolbar, selectSave.The project is saved to the same location from which you opened the project.
- From the toolbar, select the down arrow after, select Save As, and then inSave project as, complete:- Name. Enter the new name of the project.
- Location. Type the path where you want to save the project. Select and browse a folder to navigate to the location.
- (optional)Use Version Control. Select to track changes made to the project and store the project in a Git repository.TIP: In order to use version control, FactoryTalk Optix project names and repository names must match. The project and repository names must contain only alpha numeric characters, numerals, periods, dashes, and underscores.
- (optional)Encrypt secrets. Select to encrypt sensitive data contained in projects.
 
- From the toolbar, select .The project is saved and a commit is made to the local version control repository.
repository
network drive
removable drive
    
Provide Feedback