Project secrets encryption
    Encrypt sensitive data contained in projects within a specific organization.
Requirements
      To encrypt project secrets, while creating a project or saving an existing project:
        
- Log on toFactoryTalk HubinFactoryTalk Optix Studio.
- Be a part of an organization.
- SelectEncrypt secrets.
Encryption scope
      FactoryTalk Optix
:
        - Encrypts passwords in projects.
- Encrypts custom objects with the Password DataType.
- In the projectYAMLfiles, which represent the project information model, replacesValuenodes withSecretValuenodes with encrypted text values.
Projects with encrypted secrets
      FactoryTalk Optix
 handles encrypted projects in a variety of ways:
        - Opening an encrypted project when you do not have access to the organization used to create the project blanks all project secrets.
- Saving an encrypted project as an unencrypted project removes all secrets.TIP: User passwords are not considered secrets and are not encrypted with FactoryTalk Hub key.
- Deploying an encrypted project to an unencrypted client displays a warning message. For more information, see Project encryption on a client device.
- Pasting an object from an encrypted project to an unencrypted project blanks the secrets.
- Adding an object to the Template Libraries in an encrypted project blanks the secrets.
- Pasting a password as a text to the clipboard is disabled in encrypted projects.
encryption
    
Provide Feedback