Import files
    You can configure your project to use custom files such as fonts to use in your 
FactoryTalk Optix Application
.- In the main toolbar, select. Browse project files Browse project files
- InProject Files, select. Import file(s) Import file(s)
- Navigate to and select the file to import and then selectOpen.
- CloseProject Files.
Provide Feedback