Close a project
    Close a project from the Start page. 
You can have more than one project open at a time. When you open additional projects, additional instances of 
FactoryTalk Optix Studio
 open.- From the main toolbar, select. On the Start page, select ProjectClose Project.TIP: If you open the Start page from an open project and want to close the Start page, select ProjectClose Project.TIP: If you open the Start page from an open project and want to close the Start page, select. 
Provide Feedback