Project backup
    FactoryTalk Optix Studio
 automatically creates backups of projects.Projects are automatically backed up when:
        
- You save a project
- You update a project to a more recent version ofFactoryTalk Optix Studio
- You restore a project from backup. See Restore a project.
The default location for the backup folder is:
%localappdata%\Rockwell Automation\FactoryTalk Optix\Studio\Backups\
Project Name
Each of the project folders consists of other subfolders with the following types of backups:
        
- Automatic. Three backups, performed when saving the project.
- Recovery. One backup, performed when a corrupt project is opened and repair attempted. See Restore a project.
- Upgrade. Two backups, performed when updating the project to a more recent version ofFactoryTalk Optix Studio.
backup
    
Provide Feedback