Create a node pointer
    Create a node pointer in 
Project view
 to reference to another node of the project.- InProject view, select the folder or object to contain the variable.
- InProperties, create a dynamic link to the node to point to.For more information about dynamic links, see Create dynamic links.
- (optional) expandNodePointerand complete these properties:#- Kind. The kind of the node that the node pointer targets.
- Node class. Either:- Instance
- Type
- Any
 
 
- (optional) InProperties, select, select Display name, and enter the display name. Display name, and enter the display name.
- (optional) InProperties, select, select Description, and enter the description. Description, and enter the description.
pointer
node pointer
    
Provide Feedback