Array editor
    Use the array editor to modify the values of array variables.
Array editor

| Item | Name | Description | 
|---|---|---|
|  |  Add | Adds a cell to an unconstrained array. | 
|  | Delete | Removes a cell from an unconstrained array. | 
|  | Array cells column | Lists array cells. | 
|  | Array values column | Lists editable array cell values. 
     TIP: 
     If the array lists colors, you can select the color preview to open the color selector. You can create dynamic links in cell values and make the parent array index dynamic. For more information, see Create dynamic links. | 
|  | Applybutton | Applies changes to the array values and closes the editor. | 
|  | Cancelbutton | Cancels changes to the array values and closes the editor. | 
|  | Open in tabbutton | Opens the array editor in the central pane. | 
array
array editor
    
Provide Feedback