View node references
    View references to display all of the objects in the information model that reference a node.
- InProject view, right-click the node or item and then selectShow References.
- InReferences of (name), select a location and then selectGo to ...
FactoryTalk Optix Studio
 navigates to the instance of the type. Objects referenced in a NetLogic are not shown.reference
    
Provide Feedback