Search for nodes
    Use 
Search
 in Project view
 to search for and filter project nodes in the tree structure.- InProject view, perform any of the following:- To search for project nodes, inSearch, enter a search query.
- To clear the search query, inSearch, select. 
- To filter project nodes by type, inSearch, selectand then select or clear the node types to include in the query. 
- To clear all filters, inSearch, selectand then select Clear All Filters. Clear All Filters.
 You can search for project nodes using theirNodeID, by enteringn:Node_IDFor example:n: 85/00000000000123456TIP: You can also enter just the numeric string after the "/" as your search query. The string is unique for each project node.For example:n: 00000000000123456At least 4 characters of the NodeID are required to trigger the search. You can also search bynamespaceonly, for examplen: 8/orn: 123/, with no length requirement, but this search may take more time.
search
    
Provide Feedback