Copy paths to nodes
    Copy a path to a single node or copy paths to multiple nodes.
- To copy a path to a single node:- InProject view, right-click a node.
- SelectCopy path to node.
 
- To copy paths to multiple nodes:- InProject view, while holding thekeyboard key, select multiple nodes.Ctrl
- Right-click any selected node and selectCopy paths to nodes
 
Path to node or paths to nodes are copied to the system clipboard.
Provide Feedback