Project nodes
    Use the 
Project view
 pane to create and manage the contents of a project. Project view
 displays a tree structure comprised of nodes. The nodes are objects and variables organized in folders.Search 
Project view
 to find contents without having to navigate and expand folders. Split Project view
 to see multiple areas of the project simultaneously. project view
    
Provide Feedback