Import nodes from NodeSet
    Import all nodes from a NodeSet 
XML
 file.
     TIP: 
    Import nodes from NodeSet to import all nodes from 
OPC UA Companion Specifications
 defined in a NodeSet file. For more information, see OPC UA Companion Specifications.Prerequisites
Obtain an 
XML
 file with NodeSet to import.- To import nodes from NodeSet
- InProject view, right-clickModelfolder or any of its subfolders and then select .
- Select theXMLwith NodeSet to import.
The imported nodes appear in the folder. If you import the nodes into the same location
        again, all changes to the already imported nodes are retained.
Provide Feedback