Configure the OPC UA client
    Configure advanced properties of an OPC UA client.
Prerequisites
- To configure the OPC UA client
- InProject view, select an OPC UA client.
- InProperties, configure the OPC UA client settings.- Events:- None. Listen for no events.
- All. Listen for all events.
- Alarms. Listen for alarm events only.
 
- Synchronize the Node IDs on start. Synchronize the NodeIDs of the OPC UA nodes that are imported at design time. Synchronize the NodeIDs with the same nodes on the OPC UA server to which the OPC UA client connects at runtime.TIP: If the situation on the server is not known, setSynchronize the Node IDson start toTrue.
- Max array length. The maximum number of elements in an array.TIP: If OPC UA clients have differentMax array lengthvalues, theMax array lengthvalue of the first OPC UA client is applied for all clients.
- Server endpoint URL. The communication protocol and network address of the endpoint on the OPC UA server.
- Verify server identity:- True. Accept the certificate only if the certificate is trusted.
- False. Temporarily accept the certificate even if the certificate is not trusted.
 
- Minimum message security mode:- None. The messages may be unsigned and unencrypted.
- Signature. The messages must be signed or signed and encrypted.
- Signature and encryption. The messages must be signed and encrypted.
 
- Minimum security policy:- None. The OPC UA client does not require any specific security policy.
- Basic256Sha256. The OPC UA client requires this policy or a more secure policy.
- Aes128_Sha256_RsaOaep. The OPC UA client requires this policy or a more secure policy.
- Aes256_Sha256_RsaPss. The OPC UA client requires this policy.
 
- Client certificate file. The publicDERcertificate file of the OPC UA client (X509v3).TIP: The client certificate file must be in theFTOptixApplication/ProjectFiles/PKI/Own/Certs/folder.
- Client private key file. The privatePEMkey file of the OPC UA client encoded with ASCII Base64.TIP: The client private key file must be in theFTOptixApplication/ProjectFiles/PKI/Own/Certs/folder.
- Application URI. A URI that globally identifies the application instance.
- Application name. A legible ID of the application instance, which may not be unique.
- Product URI. A URI that globally identifies the software.
- User identity type:- Anonymous. No information available on the user.
- User/Password:- Username. The name of the user.
- Password. Password of the user.
 
- Certificate:- User certificate file. The publicDERcertificate file of the user (X509v3).TIP: The public certificate file of the user must be in theFTOptixApplication/ProjectFiles/PKI/Own/Certs/folder.
- User private key file. The privatePEMkey file of the user encoded with ASCII Base64.TIP: The private key file of the user must be in theFTOptixApplication/ProjectFiles/PKI/Own/Certs/folder.
 
 
 
Provide Feedback