Configure the trusted certificates at design time
    Set up a trusted certificate at design time by importing a file that has the certificate.
- From the toolbar, select. Browse project files Browse project files
- Select a certificate and select. Import file(s) Import file(s)
- Select the certificate.For more information, see Certificates and keys location.
- SelectClose.
Provide Feedback