Edit an event logger
    You edit an event logger in the central pane and 
Properties
.Prerequisites
- To edit an event logger:
- InProject view, double-click an event logger object.
- To change the variables to log, in the editor, expand categories to select or clear variable checkboxes and then selectApply.IMPORTANT:When selecting a variable to log, a dynamic link is automatically set underEvent fields to log. The dynamic link points to the automatically selected corresponding event argument. If the event argument does not represent the data of interest, select a different attribute in theDynamic linkdialog box.You can combine multiple event arguments by using dynamic links or converters (for example, a string formatter).
- To change the event logger properties, inProperties, set:- Enabled:- True. The logger logs events.
- False. The logger does not log events.
 
- Locales. The translations of localized strings stored in the database based on the locale IDs (for example,en-US).
- Database. The database that records the logger data.
 
- To add an event configuration and log events of interest:- InProperties, next toEvent configurations, select. 
- UnderEventConfiguration, set#Event source.SourceEvent sourcevalueListen subtreevalueAny project object:(no value)TrueA node/object and all its child objects:Dynamic link (parent node/object)TrueA specific project object:Dynamic link (specific object)False
- InEvent type, select the event of interest type.TIP: Consider creating a dedicated event logger for audit event types.
- In the central pane, select the variables to log and selectApply.IMPORTANT:When selecting a variable to log, a dynamic link is automatically set underEvent fields to log. The dynamic link points to the automatically selected corresponding event argument. If the event argument does not represent the data of interest, select a different attribute in theDynamic linkdialog box.You can combine multiple event arguments by using dynamic links or converters (for example, a string formatter).
- To log only the events generated by user interactions with the application, setNon-interactive sessions excludedtoTrue.
 
- To delete an event configuration and stop logging specific events, inProperties, next toEventConfiguration, select#.Delete
Provide Feedback