Logger
    A logger object records data and stores it in a database.
These logger types are available:
      
- Data logger. Samples values of one or more variables at regular time intervals or on demand.
- Event logger. Records the properties of one or more event types generated by:- A specific node and/or its child nodes
- Any node in the project
 
database
    
Provide Feedback