Import a template
    Place a template in a node in 
Project view
 to add the object, object type, or a variable to the project.
     TIP: 
    If the template is a graphic object, you can drag the graphic element from the library to the editor.
- From the main toolbar, selectand either:Template Libraries- Drag a template from the library into a node inProject view.
- Drag a graphic object template fromLibrariesto the editor orProject view.
 
- If the template is an object type, select either:- Import as type. Add an object type based on the template into the project.
- Import as instance. Add an object instance based on the template into the project.
 
import
type
instance
    
Provide Feedback