Create a library folder
    Create a folder in a local or remote library to organize the templates that belong to that library.
- From the main toolbar, select.Template Libraries
- Select a library in which you want to add a folder.
- InTemplate Libraries, selectand select New folder. New folder.
- (optional) Enter a name for the folder.
New folder appears under the selected library in 
Template Libraries
.library folder
local
    
Provide Feedback