Communicate with Azure IoT Hub broker
    Azure IoT Hub supports sending or receiving information only on specific topics of a device.
Prerequisites
Azure IoT Hub does not allow you to send and receive information on custom topics. A device can send or receive information only on specific topics of the device:
- send
- devices/deviceid/messages/events/
- receive
- devices/deviceid/messages/devicebound/#
- To communicate with Azure IoT Hub broker
- For each client that to send or receive messages, create a device on the Azure IoT Hub.TIP: Clients cannot use the same devices to send or receive data.
- Verify that sending and receiving messages is successful.TIP: The Device Explorer and Azure IoT Explorer applications enable you to monitor the received messages and send messages to devices.
Provide Feedback