Apply a global style to the project
    Select a style sheet for a 
FactoryTalk Optix Application
 to display at runtime.Prerequisites
- Configure a global style in a stylesheet. See Configure a style sheet.
- To apply a global style to the project
- InProject view, select eitherNativePresentationEngineorWebPresentationEngine.
- InProperties, inStyle sheet, select the drop-down arrow after the style sheet value and then select the style sheet to apply.
The project uses the 
Global Style
 properties from the selected style sheet.Provide Feedback