Draw a line
    Use the 
Line
 tool to draw a line.- InProject view, double-click the container to include the object.
- In the editor toolbar, selectLine.
- In the editor, position the crosshair where the line, polyline, or polygon is to begin.
- Drag to draw the line.
The object appears in the editor and in 
Project view
.Provide Feedback