Configure a video
Insert a video file container to your project, and place a video file in it. Use video files local to the project or remote videos.
- InProject view, inUI, right-click a container and then select .
- InPath, either:
- SelectBrowseand select the local video to display.TIP:To find items, start typing the item name to find inSelect file.If the file does not appear inSelect file, selectand in
Import file(s)Import file(s), select the file to import and then chooseSelect. - Enter the address of the remote video file to display.
- (optional) Set the auto play options.
- Auto play. Video will be played automatically. Disabled by default.
- Muted. Video will play without sound. Disabled by default.
- Loops. Specifies the number of times video will play. The default is1.
- (optional)Muted.
- (optional) Set theAppearanceandSize and layoutproperties.
Provide Feedback