PDF Viewer
    Displays a PDF file at runtime.
Operation
      The PDF viewer can display either:
        
- A local PDF file stored in the project directory
- A PDF file stored on a remote serverPDF viewer supports these protocols for displaying remote PDF files:- http
- https
 
Use case
      Use embedded PDFs to provide the end users with quick access to technical documentation.
Provide Feedback