Window
    Root container. In a Presentation Engine, you can set Window to specify the initial user interface at runtime.
Use case
      Window must be present in each project. Window is an object type and cannot have instances. The Window object contains all of the objects in the user interface and the logic of those objects.
        
    
    
     TIP: 
    
You can create multiple Window objects to use with different presentation engines. See Presentation engines.
The 
X
, Y
, and Always on Top
 properties apply only to the Native Presentation Engine.Provide Feedback