Momentary button
    Generates events to perform methods. Includes Minimum hold time and Maximum hold time properties.
Events
      Use these button events to trigger methods:
        
  
    
| Event | Generated at runtime when | 
|---|---|
| MouseClick event | An object is clicked or touched and then released. | 
| MouseDown event | An object is clicked or touched. Use these methods to configure the behavior of the MouseDown event:
                     
 | 
| MouseUp event | The click or touch of the object is released. | 
Example
      Default momentary button

Provide Feedback