Delayed button
    Generates events to perform methods. Includes a MouseLongPress event.
Events
      Use these button events to trigger methods:
        
  
    
| Event | Generated at runtime when | 
|---|---|
| MouseLongPress event | An object is clicked or touched for the time specified in the  Delayproperty. | 
| MouseClick event | An object is clicked or touched and then released. | 
| MouseDown event | An object is clicked or touched. | 
| MouseUp event | The click or touch of the object is released. | 
Example
      Default delayed button

Provide Feedback