Button
    Generates events to perform methods.
Events
      Use these button events to trigger methods:
        
  
    
| Event | Generated at runtime when | 
|---|---|
| MouseClick event | An object is clicked or touched and then released. | 
| MouseDown event | An object is clicked or touched. | 
| MouseUp event | The click or touch of the object is released. | 
Use case
      Trigger different actions, for example:
        
- Start report generation
- Acknowledge active alarm
- Signal an emergency condition
Example
      Three buttons with different styles

Provide Feedback