Enable or disable a graphic object
    Enable or disable an object. At runtime, users can interact with enabled objects.
- InProject viewor in the editor, select the object to enable.
- InProperties, inEnabled, select either:- True. The object allows user interaction at runtime.
- False. The object prevents user interaction at runtime.
 
Provide Feedback