Edit graphic object properties
    Change the properties of an object to change the name, unique properties for the object, as well as its appearance and behavior at runtime.
- InProject viewor in the editor, select the object to edit.
- InProperties, edit the properties values.TIP: The displayed properties for an object depend on the selected object. See Common properties.
(optional) In 
    
    
Events
, add methods to run when an event occurs. See Add a method to an existing event.
        
     TIP: 
    Gauge objects contain 
Value
 and Gauge
 categories. If the Minimum value
 and Maximum value
 properties of a gauge change continuously and rapidly, the performance of the runtime application is impacted because the gauge must be redrawn with each change.Provide Feedback