Remove a dynamic link
    Remove a dynamic link from a property to no longer have the property display the linked attribute. After removing the dynamic link you can reset the default value for the property.
Prerequisites
      
    - To remove a dynamic link
- InProject viewor the editor, select the graphic object that contains the property with the dynamic link.
- InProperties, in the property that contains the dynamic link, right-click the dynamic link and selectRemove link.The dynamic link is removed from the property and the value entered for the property appears.
- (optional) Right-click the property value and selectReset value.The property displays its default value.
Provide Feedback