Enable PowerFlex tags in a project
    - In Project view, selectDriveConnectionDesignTimeNetLogicand in Properties, set up the following PowerFlex parameters:- Update rate
- IPAddress
- PFType
 
- To create a PowerFlex model, right-click onDriveConnectionDesignTimeNetLogicand execute the GetPowerFlexModel method.The model is available in a new directory named with the PowerFlex type, its IP address, and update rate. For examplePF755TM_10.76.38.210_10sec.
- To add another PowerFlex drive, repeat steps 1 and 2.
Provide Feedback