CREATE clauses
    CREATE
 statements partially support TABLE
 and INDEX
.
     IMPORTANT: 
    
CREATE
 statements, including TABLE
 and INDEX
, are not supported by the Influx database parser. Only explicit schema can be managed or modified using client API. For more information, see https://docs.influxdata.com/influxdb/cloud/admin/buckets/bucket-schema/.Examples
      CREATE UNIQUE INDEX Table_Index ON Table1 (Column1)
CREATE INDEX IF NOT EXISTS Table_Index ON Table1 (Column1)
CREATE TABLE TempTable AS SELECT Column1 FROM MyTable WHERE Column1 > 5
CREATE TEMPORARY TABLE TempTable AS SELECT Column1 FROM MyTable WHERE Column1 > 5
Provide Feedback