Create an ODBC database
    Create a database object that fetches data from an SQL server or a MySQL server.
Prerequisites
To connect to an ODBC database from 
Windows®
 devices:
        - Install one of these ODBC drivers:- MySQL Unicode
- ODBC Driver 17 for SQL Server
 
- Configure the ODBC data source. See Administer ODBC data sources - Microsoft Support.
- InProject view, right-clickDataStoresand selectODBC database.
- InProperties, inDBMS type, select the type of the database server.
- InProperties, complete:- DBMS type. EitherSQL ServerorMySQL.
- (optional)DSN(Data Source Name). Applicable only forWindowsdevices.IMPORTANT:If specified, the DSN automatically provides the ODBC connection properties.You cannot overwrite the DSN properties by manually completing theServer,TCP Port,Database,Username, andPasswordfields.
- Server. IP address or hostname of the database server.
- TCP Port. TCP port of the database server.NOTE: The default 0 value resolves to 1433 for SQL servers and 3306 for MySQL servers.
- Database. Database name in the database server.TIP: Providing the database name is optional if the database name is specified in the ODBC connector.
- Username. Name of the user that can access the database.
- Password. Password of the user that can access the database.
 
(optional) Configure the database structure. See Configure a database table.
Provide Feedback