Read/write operation codes
    For each read/write operation of a single or multiple tags, the controller generates an operation code that describes the operation result.
Operation codes description
      
  | Code | Description | 
|---|---|
| Good | The read/write operation succeeded. | 
| BadNoCommunication | The read/write failed because of a timeout, such as a connection timeout. The  Timeoutproperty value of a Communication stationdetermines the timeout. | 
| BadCommunicationError | The read/write operation failed because the controller returned an error. | 
| BadConfigurationError | The read/write operation failed because of a tag configuration error such as an invalid address. | 
Read operation codes in C#
      You can read the operation codes in NetLogics. If the returned value is 
0
, the communication is good. If the returned value is different than 0
, the communication is down.Example:
        
var station = Project.Current.Get<Station>("CommDrivers/RAEtherNet_IPStation1");var stationState = station.OperationCode
Provide Feedback