OMRON Fins Driver
    Observe these guidelines when working with the OMRON Fins Driver.
Supported controllers
      The driver supports OMRON® CJ and CP controller families.
     IMPORTANT: 
    The driver has been tested with CJ2 controllers family.
Controller tags import
      You can only import tags from TXT files in the offline mode. 
     IMPORTANT: 
    
Before you import tags into 
FactoryTalk Optix Studio
, from CX-Programmer, copy the symbol table into a TXT file.For more information, refer to the product documentation.
Data types
      
  | Controller data type | FactoryTalk Optixdata type | Length | |
|---|---|---|---|
| BOOL | BOOL | 1 BIT | |
| CHANNEL | INT16 | 2 BYTES | |
| COUNTER | INT16 | 2 BYTES | |
| WORD | UINT16 | 2 BYTES | |
| DWORD | UINT32 | 4 BYTES | |
| LWORD | UINT64 | 8 BYTES | |
| INT | INT16 | 2 BYTES | |
| DINT | INT32 | 2 BYTES  | |
| UINT | UINT16 | 2 BYTES | |
| UINT_BCD | UINT16 | 2 BYTES | |
| UDINT | UINT32 | 4 BYTES | |
| UDINT_BCD | UINT32 | 4 BYTES | |
| LINT | INT64 | 4 BYTES | |
| ULINT | UINT64 | 8 BYTES | |
| ULINT_BCD | UINT64 | 8 BYTES | |
| REAL | FLOAT | 4 BYTES | |
| LREAL | DOUBLE | 8 BYTES | |
| TIMER | INT16 | 2 BYTES | |
| STRING | STRING  |  LENGTH | |
| ARRAY 1 dimensional | Type [dimension] | 
|  Controller memory area | FactoryTalk Optixmemory area |  Notes | 
|---|---|---|
| CIO | CIO area | |
| A | Auxiliary area | |
| T | Timer | |
| C | Counter | |
| D | Data Memory | |
| H | Holding area | |
| W | Work area | |
| Ex | EM area CurrentBank | Addresses memory location x in the current bank. | 
| Ex_y | EM area | Addresses memory location y in bank x. | 
| IR | Not supported | |
| DR | Not supported | |
| TK | Not supported | 
Provide Feedback