Modbus driver
    Observe these guidelines when working with Modbus controllers.
Protocols
      The Modbus communication driver supports these protocols:
        
- Modbus TCP. TCP Socket access mode.
- Modbus RTU. Serial port access mode.
Data types
      The Modbus communication driver supports these data types:
        
  
    
| Data type | Length | 
|---|---|
| Bool | 1 bit | 
| Byte | 1 byte | 
| SByte | 1 byte | 
| UInt16 | 2 bytes | 
| Int16 | 2 bytes | 
| UIn32 | 4 bytes | 
| Int32 | 4 bytes | 
| Uint64 | 8 bytes | 
| Int64 | 8 bytes | 
| Float | 4 bytes | 
| Double | 8 bytes | 
| String | 80 characters by default | 
| Array | 
Data areas
      The Modbus communication driver supports these data areas:
        
  
    
| Area | Modbus Function Code (Hex) | Addressing | Data Type | Access | Ranges | 
|---|---|---|---|---|---|
| Single Coils | 01 Read 05 Write (Single) | Coil Status | Boolean | Read/Write | 0-65535 | 
| Coils | 01 Read 15 Write (multiple) | Coil Status | Boolean | Read/Write | 0-65535 | 
| Discrete Inputs | 02 Read | Input Status | Boolean | Read Only | 0-65535 | 
| Single Register | 03 Read 06 Write | Holding Register | Word | Read/Write | 0-65535 | 
| Multiple Register | 03 Read 10 Write | Holding Register | Word | Read/Write | 0-65535 | 
| Input Register | 04 Read | Input Register | Word | Read Only | 0-65535 | 
     TIP: 
    The addressing may differ from device to device. For more information, refer to the device documentation.
Provide Feedback