Alarm grid
    Use the 
Alarm grid
 widget to display and manage alarms at runtime. View alarm information, acknowledge, confirm, shelve and unshelve the alarms.
     TIP: 
    The 
Alarm log grid
 widget displays alarm events recorded by the configured event logger, such as the Alarm History Grid
. Use the Alarm History Grid with filter
 widget to filter logged data.Overview
      Each row in the grid indicates a change in alarm status. Acknowledge and confirm one or all alarms on the grid. The 
    
Alarm grid
 widget displays these columns of information:
        
  | Column | Description | 
|---|---|
| Timestamp | Date and time of the last alarm event update. | 
| Name | Name of the alarm object that generated the alarm event. | 
| Source variable | Variable the event monitors. | 
| Message | Message associated with the alarm event. | 
| Active | Whether the alarm is:
                    Inactive  Active | 
| Acked | Whether the alarm is acknowledged or unacknowledged:
                    Unacknowledged  Acknowledged | 
| Confirmed | Whether the alarm is confirmed or unconfirmed:
                    Unconfirmed  Confirmed | 
| Severity |  Level of alarm severity from 1 to 1000.  | 
Runtime
      You can show or hide the grid columns at runtime, see Manage data grid columns at runtime.
        
Provide Feedback