Applications

The Applications page displays all the applications affiliated with an organization.
To view the Applications page, from the FactoryTalk menu, select
Applications
.
Applications are displayed as tiles. FactoryTalk Hub tiles are arranged by sections that only appear if you have access to an application that would be in that section. For example, if you have not made any applications favorites you do not see a favorites section. There is also information and interactivity associated with each tile.
FactoryTalk Hub Tiles and Badges
Graphic shows types of tiles and badges available in FactoryTalk Hub
FactoryTalk Hub Tiles and Badges
Tile Type or Badge
Description
Notes
Tile Sections:
Pending for (Org Name)
Tiles for not provisioned services and for which the logged in user is an Admin or Owner for the organization and has active unallocated entitlements for the service.
This section only appears for administrators and owners of the organization.
Favorites
Tiles marked by the user as Favorites.
For you
Displays the tiles for applications that are already provisioned for the organization, and the user has access and can open them.
By request
Displays the tiles for applications that are provisioned for the organization but the user does not have access to them and cannot open them. The user must request access from the administrator.
More from Rockwell Automation
Displays the rest of tiles for all other applications available in FactoryTalk Hub that are not provisioned for the organization or are available for preview only.
Icon on tiles:
Star on tile
A filled star indicates that the user has marked it as a favorite. Once marked, the tile will also appear in the favorites section of FactoryTalk Hub.
The star appears empty if the application is not selected as a Favorite
Purple icon with number inside
Indicates the number of entitlements the user has available to allocate for that service.
Only appears to Admins or Owners of the organization.
Red icon with exclamation point inside
  • If it appears in a tile that shows the button
    Set up
    in the "Pending for [org_name]" section, it tells the Admin or Owner that they must complete the custom provisioning for that service to enable the application for the rest of the users in the organization.
  • If it appears in a tile that shows the
    Open
    button in the "For you" section of the FactoryTalk Hub screen, it means all the allocated entitlements for the service are now expired or canceled. New entitlements must be allocated to have access to all the features of the app.
The purple icon cannot appear when this icon is displayed.
Action buttons on tiles:
Add+
Opens View Entitlements screen.
Appears when the logged in user is an Admin or Owner for the organization and has active, unallocated entitlements for the service.
Request
Appears on the tiles visible in the
By request
section if the user does not have access to a specific application. By selecting the
Request
button, the user requests access.
Open
Opens the application in a new tab
Product info
Opens a a pop-up with the product description
Set up
Opens the application to complete provisioning workflow.
The logged in user must be an Admin or Owner of the organization.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal