The expanded Allen-Bradley Bulletin 100-E energy-saving IEC contactor line from Rockwell Automation can help industrial companies save energy and reduce engineering time.
With new sizes from 9 to 96 A, these contactors save energy by reducing inrush apparent power (VA) by up to 68% and sealed VA by over 75% compared to standard, non-electronic coils. The electronic coils also save engineering time by covering 20 to 500 V AC/DC coil voltages with only four coil options, greatly simplifying selection.

Click to download image.
The contactors allow coil input terminals to be moved from the line to load side of the contactors without disassembly. This can make wiring and access easier when building starter assemblies. The contactors also offer a direct PLC interface option for contactors above 100A, as well as a full line of accessories, safety versions and reversing contactors.
All Allen-Bradley contactors are tested in combination with relevant motor overload relays and circuit breakers to provide two- or three-component motor starters. Using the online Global Short-Circuit Current Rating tool, users can obtain documentation certifying the compliance of specific product combinations to IEC and UL standards.
Allen Bradley and Rockwell Automation are trademarks of Rockwell Automation Inc. Trademarks not belonging to Rockwell Automation are property of their respective companies.
Published February 4, 2021